Introduction to Pressure Transducers |
What is a pressure transducer? A pressure transducer is a transducer that converts pressure into an analog electrical signal. Although there are various types of pressure transducers, one of the most common is the strain-gage base transducer. The conversion of pressure into an electrical signal is achieved by the physical deformation of strain gages which are bonded into the diaphragm of the pressure transducer and wired into a wheatstone bridge configuration. Pressure applied to the pressure transducer produces a deflection of the diaphragm which introduces strain to the gages. The strain will produce an electrical resistance change proportional to the pressure.
|
The Electrical Output of Pressure Transducers |
Pressure transducers are generally available with three types of electrical output; millivolt, amplified voltage and 4-20mA. Below is a summary of the outputs and when they are best used.
|
Millivolt Output Pressure Transducers
Transducers with millivolt output are normally the most economical pressure transducers. The output of the millivolt transducer is nominally around
30mV. The actual output is directly proportional to the pressure transducer input power or excitation.
If the excitation fluctuates, the output will change also. Because of this dependence on the excitation level, regulated power supplies are suggested for use with millivolt transducers. Because the output signal is so low, the transducer should not
be located in an electrically noisy environment. The distances between the transducer and the readout instrument should also be kept relatively
short.
|
Voltage Output Pressure Transducers
Voltage output transducers include integral signal conditioning which provide a much higher output than a millivolt transducer. The output is
normally 0-5Vdc or 0-10Vdc. Although model specific, the output of the transducer is not normally a direct function of excitation. This means
unregulated power supplies are often sufficient as long as they fall within a specified power range. Because they have a higher level output
these transducers are not as susceptible to electrical noise as millivolt transducers and can therefore be used in much more industrial
environments.
|
4-20 mA Output Pressure Transducers
These types of transducers are also known as pressure transmitters. Since a 4-20mA signal is least affected by electrical noise and resistance
in the signal wires, these transducers are best used when the signal must be transmitted long distances. It is not uncommon to use these transducers
in applications where the lead wire must be 1000 feet or more.
|
Styles of Pressure Transducers
|
PC Board Mountable Pressure Transducers
PC board mountable pressure transducers are generally compact economical pressure transducers designed to mount on an electrical
PC board and be integrated into other products.
|
|
General Purpose Transducers
General purpose pressure transducers are the most common since they are designed to fit the broadest set of applications.
|
|
Heavy Duty/Industrial Pressure Transducers
Heavy Duty/Industrial Pressure transducers feature a much more rugged enclosure than other transducers. They are designed to accommodate
heavy industrial environments. They also often feature a scalable 4-20mA output that provides much greater immunity to electrical noise which is
not uncommon in industrial environments.
|
|
High Stability/High Accuracy Pressure Transducers
Most pressure transducers feature an accuracy of 0.25% of full scale or higher. High stability and high accuracy pressure transducers can
offer errors as low as 0.05% of full scale, depending on model. Although more expensive than general purpose transducers, they may be
the only option if high precision is required.
|
|
Flush Diaphragm Pressure Transducers
With flush diaphragm pressure transducers, the diaphragm is flush to the process. This eliminates a cavity above the diaphragm that could
collect fluid matter from the process. In certain applications, this may be very undesirable. Those applications include monitoring the pressure
of foods or liquids that have very high viscosity.
|
|
Special Purpose Transducers
OMEGA offers a variety of pressure transducers with special features. These include pressure transducers designed for pressure measurement
in very high or low temperatures, submersible pressure transducers, barometric pressure transducers and pressure transducers with digital communications output
or wireless outputs.
|
|