omega-qr-code OMEGA微信公众号
咨询热线 400-820-0559

Current Multiplexer

DRA-CSM-1

Current Multiplexer | DRA-CSM-1

Current Multiplexer

¥7,073.01 DRA-CSM-1

1年保修
  • Multiplexes Sixteen 4-20 mA Inputs Into One 4-20 mA Output
  • ± 0.01% Accuracy
  • Channel Selection Controlled by 4 Discrete Inputs
  • Solid-State Technology
  • Economical PLC Upgrade

产品描述

The DRA-CSM-1 Current Multiplexer is a solid state multiplexer capable of transferring the selected 4-20 mA input current signal to the output terminals in less than 10 microseconds at an accuracy better than 0.01%. The DRA-CSM-1 is typically controlled by a PLC thereby obtaining full data synchronization. The DRA-CSM-1 is provided with a unit enable/disable control line which enables the parallel connection of several multiplexers to the same controller input. The period during which the unit is disabled is used for self-testing according to a self-test procedure which checks the unit’s hardware. Model DRA-CSM-1 is powered by an external DC power supply. Each two-wire 4-20 mA transmitter is connected to the input terminals. Each channel provides a current limited voltage supply for the connected two-wire transmitter. The channel selected by the multiplexer is directed to the control device’s (e.g., PLC’s) analog inputs. Power is maintained by the multiplexer to the unselected channels thereby maintaining uninterrupted transmitter current flow. Each 4-20 mA input channel on the multiplexer has its own red LED status light which illuminates on presence of current in the loop.
订购 所有价格均为人民币税前价格,不包括13%增值税和运费!(指定型号)
网上下单立享5%折扣!

其他客户同时购买: 这个图标可以点击扩大,跳出的清单包括了其他客户在购买此产品时同时购买的其它产品。

产品编号产品描述
数量
产品描述
Quick Ship
  
DRA-CSM-1
¥7,073.01
货期: 2 周
 
Current multiplexer
Quick Ship
Click to expand/minimize a list of what others bought with theiDRN-PS-1000
iDRN-PS-1000
咨询  
货期: 
 
 
Power supply, 95-240 Vac input, 24 Vdc @1A output
所有金额以RMB显示
注: Comes with complete operator’s manual.
400-820-0559