Accessibility  Skip navigation  Site Map  Help  Search field  View shopping cart  View shopping cart  Skip to Navigation
800-819-0559 (Landline) | 400-619-0559 (Cell)
Home >> Temperature Products >> Indicating Labels, C... >> OMEGAMARKER™ T... >> OMEGAMARKER™ Series

OMEGAMARKER™ Custom Temperature Test Kit Select-a-Kit  - Discontinued

OMEGAMARKER™ Series   
 
Temperature Marker
OMEGAMARKER™ Series:OMEGAMARKER™ Custom Temperature Test Kit Select-a-Kit™  - Discontinued
Click for larger image.
   
To Order Specify OMEGAMARKER-Custom- (List Ranges)
Kit includes 10 crayons, holder, and case

View related products - Indicating Labels, Crayons, Cements and Lacquers

Click to scroll below to order See Specs PDF View a printer friendly page

The OMEGAMARKER series has been discontinued. Please contact our Temperature Engineering department.

For added convenience and versaility OMEGA offers these Temperature Test Kits. The OMEGAMARKER crayon is easy to use, but certain conditions must be considered. OMEGAMARKERS will not make any mark on smooth or rough surfaces in cold conditions. When rubbed hard on a rough surface, the OMEGAMARKER gets ground and the powder is deposited on the surface which appears like a mark, but will not adhere. The correct way of using OMEGAMARKERS would be to strike it across a pre-heated surface during the heating process, using proper safety precautions. While the temperature is below the rated temperature there will not be a visible mark, but as soon as the surface reaches the rated temperature of the marker, at the point of contact the marker will melt and make a visible mark on the surface. This is an indication that the surface has reached the rated temperature of the OMEGAMARKER.

Each of the four kits contains 10 crayons. Three kits have pre-selected values. The fourth, the custom kit, has values that can be selected by the user.

Full Range Kit

°F: 125 200 250 300 350 425 500 575 650 750
°C:  52   93 121 149 177 218 260 302 343 399

Low Range Kit

°F: 125 150 175 200 225 250 275 300 325 350
°C:  52   66  79   93 107 121 135 149 163 177

High Range Kit

°F: 300 350 400 450 500 550 600 650 700 750
°C: 149 177 204 232 260 288 316 343 371 399

Custom Kit, Select 10 Crayons from among:
Deg. F Deg. C Deg. F Deg. C Deg. F Deg. C Deg. F Deg. C Deg. F Deg. C
100 38 200 93 294 146 392 200 550 288
104 40 203 95 300 149 400 204 554 290
109 43 206 97 302 150 410 210 572 300
119 48 212 100 306 152 413 212 575 302
122 50 213 101 311 155 419 215 600 316
125 52 219 104 313 156 425 218 650 343
131 55 225 107 320 160 428 220 662 350
140 60 230 110 325 163 437 225 700 371
150 66 239 115 329 165 446 230    
158 70 248 120 338 170 450 232    
163 73 250 121 344 173 455 235    
167 75 256 124 347 175 463 239    
169 76 257 125 350 177 475 246    
175 79 263 128 356 180 482 250    
176 80 266 130 363 184 488 253    
182 83 269 132 374 190 500 260    
185 85 275 135 375 191 518 270    
188 87 284 140 383 195 525 274    
194 90 288 142 388 198 536 280    
Order on www.omegaengineering.cn and 5% will be discounted when you checkout.
  To Order (Specify Model Number)
All list prices are pre-VAT rate not including tax and shipping
 
 Part Number   Availability   Price(RMB)   Description    Qty.
 OMEGAMARKER-CUSTOM-*    Consult sales   Custom Kit (Specify 10 crayons at specified temperatures in Comments just before placing your order)  
 Crayon Kits with Degree C Crayons
 OMEGAMARKER-CUSTOM 130 130 140    Consult sales   Kit includes 10 crayons in the following Degree C: 130 130 140 140 150 150 155 155 165 165 C  
 OMEGAMARKER-CUSTOM-10 KIT DEGC    Consult sales   Kit includes 10 crayons in the following Degree C: 43, 48, 52, 55, 60, 66, 70, 75, 79, 83 C  
 Crayon Kits with Degree F Crayons
 OMEGAMARKER-CUSTOM-109/119/122    Consult sales   Kit includes 10 crayons in the following Degree F: 109, 119, 122, 125, 131, 140, 150, 158, 167, 176F  
 OMEGAMARKER-CUSTOM-119,125,131    Consult sales   Kit includes 10 crayons in the following Degree F: 119, 125, 131, 140, 150, 158, 163, 167, 175, 250F  
 OMEGAMARKER-CUSTOM-122,158,167    Consult sales   Kit includes 10 crayons in the following Degree F: 122, 158, 167, 212, 302, 392, 482, 572, 662, 700F  
 OMEGAMARKER-CUSTOM 169,175,182    Consult sales   Kit includes 10 crayons in the following Degree F: 169, 175, 182, 185, 188, 194, 200, 203, 206, 213F  
 OMEGAMARKER-CUSTOM 169,182,194    Consult sales   Kit includes 10 crayons in the following Degree F: 169, 182, 194, 206, 219, 231, 244, 256, 269, 282F  
 OMEGAMARKER-CUSTOM-206/212/213    Consult sales   Kit includes 10 crayons in the following Degree F: 206, 212, 213, 219, 225, 230, 239, 248, 250, 256F  
 OMEGAMARKER-CUSTOM 212F212 212    Consult sales   Kit includes 10 crayons in the following Degree F: 212, 212, 212, 212, 212, 212, 212, 212, 212, 212F  
 OMEGAMARKER-CUSTOM 269,275,284    Consult sales   Kit includes 10 crayons in the following Degree F: 269, 275, 284, 288, 294, 300, 302, 306, 311, 313F  
 OMEGAMARKER-CUSTOM 213F/219F    Consult sales   Kit includes 10 crayons in the following Degree F: 213F, 219, 225, 230, 239, 239, 239, 239, 239, 239F  
 OMEGAMARKER-CUSTOM 275,275,275    Consult sales   Kit includes 10 crayons in the following Degree F: 275, 275, 275, 329, 329, 329, 374, 374, 374, 374F  
 OMEGAMARKER-CUSTOM-302F,302    Consult sales   Kit includes 10 crayons in the following Degree F: 302 F (10 Crayons)  
 OMEGAMARKER-CUSTOM-392F,392,    Consult sales   Kit includes 10 crayons in the following Degree F: 392 F (10 Crayons)  
 OMEGAMARKER-CUSTOM 425 450 475    Consult sales   Kit includes 10 crayons in the following Degree F: 425, 450, 475, 500, 525, 550, 575, 600, 650, 700  
 OMEGAMARKER-CUSTOM 450,455,463    Consult sales   Kit includes 10 crayons in the following Degree F: 450, 455, 463, 475,482,488, 500, 518, 525, 536F  
 OMEGAMARKER-CUSTOM 518,525,536    Consult sales   Kit includes 10 crayons in the following Degree F: 518, 525, 536, 550, 554, 572, 575, 600, 650, 662F  
Price are shown in RMB.

 Note: Contact Sales Dept to order OMEGAMARKER-CUSTOM with 10 selected temperature crayons. Price is $74.00
(OPTIONS SHOWN IN THIS "NOTE" ABOVE ARE PRICED IN US$)

Ordering Example: OMEGAMARKER-CUSTOM-150/200/300/300/325/325/325/350/350/400F, OMEGAMARKER™ custom kit containing 10 crayons at specified temperatures in °F, $74.

   
Keywords:Low Cost Ten Crayon Temperature Test Kits OMEGAMARKER-LOW, OMEGAMARKER-HIGH, OMEGAMARKER-FULL, OMEGAMARKER-CUSTOM, ethernet temperature probe

   Back to top Back to top